Hi, E2E support
I would like to ask about DLPC3479 and DLPC4710LC.
My customer is developing on a following environment.
Controller : DLPC3479
DMD : DLPC4710LC
Light Controll : Internal Pattern Streaming Mode or Splash Pattern Mode
If Parallel Interface is not used, should user input clock pulse as PCLK ?
If yes, would you please tell me the frequency of the PCLK.
Best Regards,
Koike