Other Parts Discussed in Thread: DLPC410, DLPC900
I don't have much experience in developing the DLP device, so I got a few questions.
I want to play thousands of images(1080x1920 BMP) on an endless loop. But I find it very hard to realize when using the application 'DLP Discovery 4100 Explorer GUI'.
Fist problem is the reading speed is very slow. It took almost 1.5 hours to load the images. And every time I stop running, it re-read the script again and I have to spend another 1.5 h on the loadings.
Second, I would like to set the play interval at about 20ms, but it can't realize the function.
Third, I have no idea how to use APPFPGA, I open the DSP file in the source files and it has the following files in it:
DDC4100.dsp
DDC4100.h.
DDC4100.cpp
DDC4100.rc
DDC4100.def
DDC4100.clw
DDC4100.odl
/////////////////////////////
DDC4100 control:
DDC4100Ctl.h
DDC4100Ctl.cpp
DDC4100Ppg.h
DDC4100Ppg.cpp
DDC4100Ctl.bmp
Is it the APPFPGA mode? Can I develop the sequence mode I need by writing codes? If I can, which file in this project can I develop?
Since I could hardly find the detailed instructions of the development, I wonder if you could provide the developing service which could assist the efficiency of our work?