Other Parts Discussed in Thread: DLPC900
Hello Team,
My customer has written some USB control software for a DLP6500 DMD controlled by a DLPC900. When they try to change video mode to "video pattern mode" they get a command failed error because video is not locked. If they first set the input source configuration to "24 bit parallel" first, then they can change the video mode. The odd part is that if read the input configuration before setting it, it is already set to "24 bit parallel" on startup. This is problematic because even though it says it is set properly, they cannot change the video mode or achieve video lock unless they set it manually anyways.
System details (read with USB commands 0x0205 and 0x0206):
Application software: 3.0
API software: 4.1e
Software configuration: 68.33
Sequencer configuration: 68.33
Hardware config: DLP6500
Firmware tag: DLPR900PROM-6500-v3.0.0
Regards,
Renan