This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP3010: Are dimensions of these flyeye lenslets manufacturable?

Part Number: DLP3010

We have an uncommon F number system where for maximum portability our illumination flyeye lenslet pitches have to be 0.2 mm. I understand the reference designs don't go smaller than 0.6mm. Any idea if our pitch size is manufacturable with diamond turning or whether it is likely impractical?

Thanks