Hi TI Support
I made the board with DLP3010+DLPC3478+DLPA3000. The operation test was conducted, and I2C communication works normally, but the LED does not turn on. Firmware was downloaded from "">software-dl.ti.com/.../" site as DLPC3478+DLPA3000_AC+Option1(Default)+0x36(default)+8.00 and used. Do I need to receive a separate firmware and use it? Or is the firmware I got from the above site valid? If it's not a firmware problem, can I get a schematic for reference? I couldn't find a schematic for the above combination. Please answer about my question. Thank you.
Looking forward to your reply.
Best regards!