This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP9000X: DLP9000X EVB

Part Number: DLP9000X

Hello,

I am designing a circuit to work with the DLP9000X. I am basing my schematics on TI EVB schematics (attached).
on those schematics, there are circuits to for the power down procedure of the DLP9000X. 

My questions are:

1. I am trying to understand each discrete circuit of the VOFFSET, VRESET, VBIAS power down on page 4(I circled them).

    1.1 VOFFSET.
          1.1.1 on normal mode the EN_OFFSET is '1' and thus Q3=ON which results in Q2=OFF and Q1 also OFF => VOFFSET working regular
          1.1.2 on power down...EN_OFFSET is '0' and thus Q3=OFF which results in Q2=ON and thus Q1=ON => VOFFSET tied to 3.3V by D1 Zener diode? until powered down?
     1.2 VRESET
          1.2.1 on normal mode the EN_OFFSET is '1' and VRESET is powered (-10V per schematics) .....Q4 is OFF?! and also Q5, Q6 ....i.e: normal operation.
          1.1.2 on power down...EN_OFFSET is '0' and thus Q4=ON (? not sure i understand why) which results results in Q6=ON and thus Q5=ON => VRESET tied to GND?
   1.3 VBIAS.
          1.1.1 on normal mode the EN_OFFSET is '1' and thus Q9=ON which results in Q8=OFF and thus Q7 also OFF => VBIAS working regular
          1.1.2 on power down...EN_OFFSET is '0' and thus Q9=OFF which results in Q8=ON and thus Q7=ON => VBIAS tied to GND?

2. based on the above. May i know why I need such transistors? 2N2222 exists only in T.H form. trying to select other SMT I find that the Collector- Base Voltage VCBO of 60 V and Emitter- Base Voltage VEBO of 6V
    determine that T.H package... why those figures were chosen. the reason i ask is that each of those transistors costs around $5...so the whole solution for power down estimates to around $20-$30 per board.... doesn't sound reasonable....