Other Parts Discussed in Thread: TEST, DLPA3005, DLP4710, DLPC3439, , DLPA3000, CSD17501Q5A, DLPDLCR3010EVM-G2, DLPDLCR2000EVM
Hi,
I want to decrease led current of dlp4710evm-g2 below of 1423ma down to 0 ma but when in dlp light crafter I was changed the led current below of 1423ma and click set button it did not set and when I click get button its value changed to 1423ma.
I test this in advanced mode but when changed value of Rgb led current and write 0 to all of them and click write button it did not set and when I click read button its value changed to 91.
Is there any solution?