Issue on the DLP6750, only half of the PLM works as shown in the attached. There should be another letter shown in the left half of the image but only right half is working right now. I set the lab power supply with 1.3V voltage, and 8 mA current limit. Some other setting in the GUI is shown as the attached screenshots.
Thanks