This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPLCR65EVM: Power Consumption

Part Number: DLPLCR65EVM
Other Parts Discussed in Thread: DLP7000, DLPC900, DLP9000, DLP9000X

Hello,

Is it possible to get approximate current consumption of the DLPLCR65EVM board. We are using this board

From the datasheet the power requirements are in Section 5.1 Nominal voltage: 12-V DC; Maximum Current: 7 A; and the recommended power supply is Digi-Key part number 102-3811-ND, which is 5A

The actual current measurement I have made was 0.48A

We are only using display port for imaging and USB for a control

Best regards,

Timur