This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP4710LC: Phase Modulation Using 4710-LC DMD

Part Number: DLP4710LC
Hello, our team is working on designing optical setup which requires DMD exposed light modulation platform that we could use to develop our optics around it.
we are looking for a small chip and were wondering if 4710 Light control is available without the optics for use of phase modulation experiment and can we stream data for projection from our computer directly to it since we need to project many patterns in sequence.
Regards,
Montello.
  • Dear Montello,  EKB Technologies Ltd offers a naked E4750-LC which is based on the 4710-LC setup . The kit is offered for developers to build their optical setup around the DMD and could be utilized for Binary phase modulation in variety of applications. 
    in case you wish to create multiple images and run them from a pc , the setup supports injection of video through HDMI which is specifically delivered without altering the data for appearance improvement vs. the standard video chipsets where data is modified for the benefit of producing better looking image to the observer.  In this case the feed will stay raw which will ensure accuracy of the projected patterning you create for the phase modulation purpose.
     
    you can find additional information on our website at: https://www.ekbtechnologies.com/e-store/pcba-with-dmd