I am using a PRO6500 from Wintech Digital which uses the DLP6500. Currently using the TI LightCrafter 6500 & 9000 GUI to control the DMD.
My pulsed laser is operating at 100 Hz with a 10% duty cycle, yet there is significant pulsing when using a bit depth of 8 on the DMD. It also appears at any bit depth above 1, but is most severe and noticeable at 8. I have not yet examined the pulsing behavior with a beam profiler yet, but have observed this behavior with visual and thermal cameras: the pulsing is quite significant and noticeable at around ~10 Hz. I am looking at the exposure time required to display a grayscale images on the DMD and it is significantly lower than the frequency of the laser, so I am confused as to why this pulsing reveals itself even when observing with cameras that operate with frame rates of 25 or 30 fps.
I am new to using this: any help or point in the right direction is appreciated!