Other Parts Discussed in Thread: DLP471TE, DLPC7540, DLP471NE, DLPC7540EVM
Hi,
I am using a DLPC7540 with a DLP471TE.
I want to use this device with 240Hz1080p.
The user guide says that this device works at 1080p with the firmware "Flash_DLPC7540_DLP471NE_LED.img".
I installed the above firmware and checked it using Nvidia-setting, and it worked for 1080p.
However, I can only select 60hz, 30Hz, and 15Hz as the refresh rate in Nvidia-setting.
Can you please tell me how to set it to 240Hz?