Other Parts Discussed in Thread: DLP3010, , DLP3010LC, DLPC3478, DLPA2005
Hello, I ask before purchasing just to be sure. According to specifications, a DMD (DLP3010, DLP .3 720p DMD) is included in the controller so no need to buy it separetely. I want to make sure it is included and also, consulting user's guide, figure 1, DMD is indicated on the top right corner, but I see a sort of flexible band in there and not the DMD (expected a silver coated rectangle). So, If someone could provide a photo of the DMD on the device it would be helpful. Also, just want to make sure it works well on visible light range (it seems like a few models have aspecific wavelenght range).
Help is appreciated.