Other Parts Discussed in Thread: DLPC3479
Hello ,
I downloaded the firmware for the DLP4710EVM-LC from the following website
www.ti.com/.../DLP4710EVM-LC
The attached release notes include the following statement
===
The firmware is primarily intended for the DLP4710EVM-LC Evaluation Module, but can be used for any DLPC3479 dual ASIC system with the following configuration:
...
- DMD Pin Mapping: Option 1
===
In "DLPU079A - Using the DLP4710EVM-LC Light Control Evaluation Module", it says "This optical module interfaces with the EVM using DMD pin mapping Option 2".
Is this a typographical error in the release notes?
Best regards,
K Hayashi