For our application we would like to image an object to the DLP and use ROIs (region of interest) to switch only the element who is interesting on a detector.
I check on your appplication (DLP LightCrafetr 6500 & 9000 - 4.0.1) to use flat-mode, but there are only "On state mode" ( +12°) and "Off state-mode"(-12°) when we use the "video mode".
Is it possible to program the DLP in the park mode or in land mode (when the mirrors are plan) for the selection and use "On state" or "off state" to unselect elements ?
We made a optical system to use DLP in plan and to use +12° or -12° to not select elements of the image.