Other Parts Discussed in Thread: DLPC230-Q1, TPS99000
Hi
I have procured a DLP 5530 EVK Kit
I have gone through the schematic and understood that the HDMI interface is done to DLPC is through chip TVP401, which is a HDMI to parallel converter bridge
what i could not understand is following things
1. How the HDMI transmitter(That is PC) is coming to know about the supported resolution of DMD kit that is 1152x1152 and 1152x576 ?
2. if i have made my own DMD board, should i need to seperately program the DLPC from host processor on startup to change the resolution ? or the DLPC understands incoming resolutions ?
3. if i have made my own DMD board, should i need to sperately program the DMD IC also from host processor or just the DLPC can take care ?
4. I can see a Flash memory tied to DLPC, will TI provide me the facility to program the DLPC to program same bin of dmd kit?