Other Parts Discussed in Thread: DLP4710EVM-LC, DLP4710, DLPC3439, DLPC3479
We aim to use the DLPDLCR4710EVM-G2 evaluation board without the LEDs. To achieve this, we tried to use a custom batch file, which disables the LEDs in the startup process. Therefore we used the GUI software "DLP LightCrafter Display" in advanced mode. We tried to execute a "Flash Image Update" without success.
When using the firmware from the Firmware Selector tool, an error occured, saying the firmware is meant for another type of EVM.
When using the firmware from the DLPDLCR4710EVM-G2 product page, the software returned immediately, that the update was successful. Despite the message saying it was successful, nothing really changed. The LEDs still turn on while starting up the EVM. We think, that no update was carried out and the batch file was not loaded to the EVM.
Can you support us creating and uploading a custom Auto-Init batch file?