This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Product Selection

Other Parts Discussed in Thread: DLPC910, DLPC900, DLP6500FLQ, DLPLCR4500EVM

Hi,

Good Day. I have a customer who has a query about DMD. Please see below 

I need one or two DMDs to use in my optical setup. 

So, I have used SLMs for my projects, but right now because of polarization interaction I need to work with DMDs. I need a DMD with at least HD resolution, pixel size around 8 micrometer and ability to do phase correction compatible with wavelengths 400-700 nm.

Also, I need the whole device, like its connecter and so on. If you have a device as described already, it will be fine. If not, how can I get such device. 

We already have one device from your company but its resolution is low, the model name is: "DLP LightCrafter Evaluation Module"

I think the model DLP6500 is compatible with my setup, but I also need to control the radiation through the controller. How can I get the entire package to use the DMD in my optical setup instead of a SLM?

Finally, the attached files are related to the DMD that we have from your company. I want the display chip as well as the rest of the package.


Best Regards,

Ray Vincent