Hello, TI expert
I am making a program to directly control Dlpc3470 through STM32duino I2C communication.
While testing, I noticed something odd.
To set the LED Current to 300mA, 0x2C (LSByte) and 0x01 (MSB) were input as parameters of Write Opcode in order.
However it was set to about 738mA.
More test results..
Multiply the current value I want to set by about 0.405, I found out that I had to put the hexadecimal number corresponding to the multiplied value as a parameter.
That is, to set LED Current to 300mA, 0x79(LSByte), 0x00(MSByte) must be input as parameters.
You would like to know why you need to enter the converted value rather than 300 (DEC) hexadecimal. I would also like to know the formula used for the conversion.
Thanks for reading the question