Hi Team,
Use the DLPLCR4500EVM to illuminate the object.
In Pattern Sequence Mode, we set the following pattern to continue with a single pattern with 60 FPS.
In this case, while the pattern is being irradiated, it is expected to be irradiated with constant brightness.
Actually, there is a brightness fluctuation of 17-18 Hz as follows.
We want to decrease the brightness fluctuation since about 10% of it would effect the measurement.
Is there any way to suppress this amount of brightness fluctuation on DLPLCR4500EVM setting?
Beat Regards,
Tom Liu