This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP3030PGUQ1EVM: The maximum current on the P12V_HC_6 network at maximum brightness of the PGU

Part Number: DLP3030PGUQ1EVM


HI,

On TI's DEMO (using Q8WP LED, what is the maximum current on the P12V_HC_6 network at maximum brightness of the PGU? I want to use this data as a reference to select a BUCK-BOOST chip to generate 12V voltage (P12V_HC_6)