Other Parts Discussed in Thread: DLP230GP, DLPC3430, DLP2010, DLPC3432, DLP230NP
Hi,
I need a small projector such as the DLPDLCR2000EVM (can be another). I have two requirements in addition to small size:
(1) Refresh rate must be high (200Hz+)
(2) Must be able to dim screen as much as possible
Don't care much about resolution, and I want *less* nits not more. Ideally I want to use a raspberry pi or a beaglebone black.
Dinis