This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP5531Q1EVM: Use case for Symbol Projection with HDMI

Part Number: DLP5531Q1EVM
Other Parts Discussed in Thread: DLP5531LEQ1EVM

Hello,

I came across this video featuring a demo of the DLP headlight, and would like to understand what solution can be used specifically to control the output - if there is a third-party controller and programme that controls and sends an HDMI feed to the DLPC230 controller? I'm currently working on a symbol projection use case, with the intended outcome similar to what is in the demo.

https://www.youtube.com/watch?v=RQQUhUCAiKM&t=100s

Also would there be a particular setting in the DLP Control Program that can adjust the image skew for projection?

Thanks!