Other Parts Discussed in Thread: DLPC900
Hi Team,
We received this inquiry from our customer.
I'm designing a volumetric display where DLP500YX DMD would be a great fit due to it's fast frame rate capability. However I would like to drive it directly from an FPGA in order to be able to stream 1 bit video at 16kHz frame rate, but I could not find documentation about the protocol used on the LVDS data input ports, as well as detailed description of some other ports. Is this information available (perhaps with some terms/conditions, or an NDA requirement)?
As far as I can tell, the DLPC900 controller can only achieve the maximum 1 bit pattern rate of 16kHz when having them pre-stored on the embedded DRAM because the video input ports have limited bandwidth..
I understand that by not using the DLPC900 controller there is a risk of damaging the DMD or shortening it's lifespan, but I am ok with that risk.
Regards,
Danilo