This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPC230-Q1: Firmware in building DLP5531Q1EVM

Genius 16490 points
Part Number: DLPC230-Q1
Other Parts Discussed in Thread: DLP5531Q1EVM,

Hi Expert,

Seeking advise on this:

I bought your DLPC230-Q1 chip and want to make a DLP5531Q1EVM board. May I ask if I downloaded its internal program directly from FLASH?

Instead of designing the circuit boards, I've already designed the circuit boards, and I'm wondering if I can just download the programs into them using DLP control software

Thank you.

Regards,
Archie A.

  • Hi Archie A.,

    Yes, you can program your custom board with the DLP Composer generated .bin file that would typically be programmed onto the EVM.

    Downloading the internal program directly from flash is an option to clone and copy the .bin onto your custom hardware.

    I have also granted you mySecureSoftware access to the following downloads in order to modify, build, and generate a new .bin file:

    • DLP Auto HUD/Headlight Gen 2 – DLP Composer for Automotive (Object)
    • DLP Auto Headlight Gen 2 - DLPC230 Embedded Software and Configuration Files