Other Parts Discussed in Thread: DLPC900
Hello,
I’m currently working with the DLPEVM9000LCR board. I’m communicating to the DLPC900 through a usb interface and using DLPC900 Programmer’s Guide (Rev. G) [Literature #: dlpu018g]. My main focus is using Pattern On-The-Fly mode and I’ve been using Sections, 2.4.4.4.1, 2.4.4.4.2, and 5.3 as examples.
Since I’m using the 9000, do I send an additional Set BMP (to 0x1A2C) between step 4 and step 5. Then load bytes to 0x1A2B and 0x1A2D, such as
Step 5: 0x1A2B | Load 504 bytes of left half of image
Step 6: 0x1A2D | Load 504 bytes of right half of image
Step 7: 0x1A2B | Load 496 bytes of left half of image
Step 8: 0x1A2D | Load 496 bytes of right half of image
?
Also, do steps 2 and 3 work the same way with the 9000?