Dears,
I have some questions about DLP3020 R/G/B LED LED Duty setup
1. Can the RGB LED duty cycle be set up to 100% (R+G+B) in one cycle, or what is the maximum it can be set to (99%, 90%)?
2. Can the duty cycle of R/G/B be adjusted by itself in one cycle? Is there a maximum limit?

Many thanks & Best Wishes
Weite
E:weite.chi@ofilm.com