I have a brand new DLP and BBBW and have followed the quickstart tutorial. I have installed the latest Debian image for the BBBW following the link in the tutorial but when I power both devices (no matter what order or both simultaneously) the display does not show anything. If I power the DLP on its own, I see the splash screen. i2cdetect -r -y 2 doesn't show the device address. Is there an additional step between installing Debian and being able to detect the device connected to the beagle?
If I navigate to /opt/scripts/device/bone/capes/DLPDLCR2000 the file dlp_lightcrafter-1.0.19.tar.gz is present. Should this be unpacked? Unpacking it didn't seem to do anything. I've read every post I think is relavent but haven't been able to resolve the issue.
I have made no modifications to the DLP or beagle.