This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPLCRC410EVM: Loading image using Python

Part Number: DLPLCRC410EVM
Other Parts Discussed in Thread: DLP9500UV, , DLPLCR95UVEVM, DLPC410
Hi, I have the assembly of DLPLCR95UVEVM and  DLPLCRC410EVM. I want to connect to DLPLCRC410EVM and load images on DLP9500UV using Python. Is that possible? Kindly guide me through.
Regards,
Lakhi
  • Hello Lakhi,

    We do not provide a Python example or wrapper for the API.  The GUI software is not intended to be production ready software, but rather a way to test that the basic functionality of the hardware is ok.  For example that images can be loaded and displayed, but not to run at the full speed the DLPC410 controller is capable of.

    Fizix