Other Parts Discussed in Thread: DLP4710, , DLPC3479, DLP3010
Hello everyone,
We have developed DLP4710 projector on the basis of DLP4710EVM-LC.
Now I need to update flash image by adding batchfile.
I can make batch file using advanced of DLP4710 GUI 2.2.0.6.
But after I update the firmware using the batch file, DLP4710 projector start up failed and GUI could not connect to the projector.
The batch file content as follows:
Is there any error I have made or whether other step is must do.
Regards,
Yang