This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPR410: DLPR410BYVA not initializing

Part Number: DLPR410

Hi,

re-opening this case

- Per previous question (sorry took time...was on vacation) here are our findings:

1. Until now on our products using the DLPR410AYVA we got the following readings:

    DMD_VERSION = 101 or 111

    DMD_TYPE = 000

2. on the boards we mounted the DLPR410BYVA we get

    DMD_VERSION = 000

    DMD_TYPE = 010

and thus, our SW indicates failures as it seeks the values of 5,7 for the version and 0 for the Type (i.e DLP9500UV)

Can you advise why? per the change notice the ID should not have changed