Other Parts Discussed in Thread: DLPA2005
During some tests I found some strange behavior. I have created an image of a checkerboard pattern with 1 fully white and 1 fully black pixel repeating. When I open the image the standard image viewer open the image windowed at a 33% zoom level. When I try to zoom in to 100%, or when I try to display the image full-screen the EVM resets and shows the DLP logo for a few seconds and then shows the color bars test-pattern. When I rerun the the the init_parallel_mode.py the system works again normally.
Why is the EVM showing this behavior?