This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP9000X: Analog signal for synchronizing with light source

Part Number: DLP9000X
Other Parts Discussed in Thread: DLPC910,

Hi Team,

Our customer would like to confirm if the analog signal for synchronizing with light source is available in DLP9000X. As I understand, light is controlled with DLPC910. Can you please confirm?

Regards,

Danilo

  • Danilo,

    This would have to be programmed by the customer in their front end.  The DLPC910 is a binary controller only, so that all gray scale functionality and illumination control must be done by the processor sending the binary patterns to the DLPC910 controller. 

    Fizix