This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPA2005: DLPA2005 keeps resetting the DLPC150 when connected to DLP2010NIR

Part Number: DLPA2005
Other Parts Discussed in Thread: DLP2010NIR, DLPC150
We referred to NIRscanNano design and software files for creating our own board including DLCP150, DLPA2005, DLP2010NIR for NIR spectroscopy application.
DLPA2005 keeps resetting the DLPC150(RESETZ low). Then DLPC150 keep resetting DMD by sending DMD_DEN_ARTZ low. I attached scope images.
Power On sequence is correct; Vofs,Vrst and Vbias reach specified values on their time. Fault shutdown occurs as all three Vofs, Vrst and Vbias falls to zero. Again it is starting the power on sequence and again resets; cycle repeats. What I observed in waveforms is first Vofs reaches its specified 10V as it should be. when Vbias and Vrst reaches its specified values at same time, suddenly Vofs falls below 10V and after few milli seconds reset occurs.
we have used the LBR2012T100K(10uH, 468mOhms, 150mA) instead of CBL2012T100M(10uH, 370mA, 1.3Ohm) as per reference design due to its unavailability reasons. Is this causing the problem? there was no such strange issue before few days on the same board; that time I was working on I2C to display test patterns. This strange problem has been coming for last few days. Can you suggest some solution.