This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP471TEEVM: XPR actuator for 4K UHD with DLP471TEEVM and DLPC7540EVM

Part Number: DLP471TEEVM
Other Parts Discussed in Thread: DLPC7540EVM, DLP471TE, DLPC7540

Hi.

I want to achieve 4K UHD with DLP471TEEVM and DLPC7540EVM.

If Flash_DLPC7540_DLP471TE_LED.img is used without XPR actuator, will the resolution of the displayed image be 1080p?
If I use DLP471TEEVM and DLPC7540EVM without XPR actuator, can I use 4K UHD with DLP471TEEVM and DLPC7540EVM?
Where can I purchase XPR actuator to use 4K UHD with DLP471TEEVM and DLPC7540EVM?