Other Parts Discussed in Thread: DLPDLC-GUI, , DLP4710EVM-LC
Hi,
In an earlier attempt to upload firmware (using the wrong GUI, powered off mid-process) I believe I have corrupted some data that allows the 4710EVM to connect via usb to the correct GUI.
The fans start when switched on but the button doesn't turn the LEDs/splash screen on (whereas it used to when purchased).
Similarly, the GUI says the unit is switched on but not connected (previous experience has shown me that is shows 'connected' after the button is pushed).
Is there a way to load the firmware (dpp3439-dual-ASIC_7.3.2.img) to the system?
I believe I can successfully upload MSP430 code (using a launchpad and supplied MSP430 software) if that helps - perhaps editing Main.c of PICO-FLA7-PAD3005... script to bypass or replace the button push, to allow connection to the GUI, and then upload as normal?
Any help would be appreciated.
Thanks