Hello Team,
Can you please tell me what is the maximum power that can be used without
damaging the modulator?
I found this information on the official website:
1) In the visible range up to 25 W/cm2 and thermally limited;
2) In IR (above 700 nm) up to 10 mW/cm2;
Values differ by a factor of more than 1000, are they correct?
Also, my customer is going to operate DLP6500 in the infrared range:
1) continuous radiation at 800 nm, source power up to 80 mW;
2) pulsed radiation 1040-1060 nm, pulse energy 1 nJ, pulse repetition rate
70 MHz, pulse duration 150 ns, source power up to 1 W.
Is this okay?
Regards,
Renan