This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP300S: Maximum illumination power for a short periode

Part Number: DLP300S


Hi!

For the DLP300S it is recommended to have at most 3W/cm² at a wavelength of 400nm to 550nm - I guess that value is for 100% on-time, is that right? If it is right, what happens if the on-time is only a very short periode (e.g. 0.5sec on, followed by 10 sec off) - can the maximum power than be higher? I'm sure it's not possible to official recommend this but I wonder what happens in such a case.

Kind regards,

Dominik