Part Number: DLP3030-Q1
Hello Guys,
I have a question about DLP3030-Q1.When I use my MCU to communicate with TMS320F28023 by SPI in order to change DLP3030's backlight brightness, though I can change it, I cannot receive the answer single(0x10 introduced in datasheet).The second question is that if I use the upper computer to control EVM, and after it I use my MCU to control it, I can correctly receive the answer signal . So, I really doubt that if the DLP3030-Q1 need to initialize the device or ohter method to enable it,but the datasheet did not introduce it.Could you please help me to solve the trouble.
Thanks!
Libo Wang