Part Number: DLPR410
The DLPR410 is listed on DLP9500's datasheet. What's the difference between these two variants?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DLPR410
The DLPR410 is listed on DLP9500's datasheet. What's the difference between these two variants?
Hello Xinyuan,
The DLPR410AYVA was superseded by the DLPR410BYVA.
The primary difference is that for the DLP650LNIR DMD one of the voltage for the Reset Driver was set to the value for the DLP9500. This fix was implemented in the B revision as well as a few other minor improvements.
If you are using it to operate a DLP9500, then there using the DLPR410AYVA is ok. If you are planning to use the DLP650LNIR DMD then the prom should be replaced with a DLPR410BYVA.
Fizix