Other Parts Discussed in Thread: DLPC350
Hi, I have encountered an issue on using the pattern sequence mode with DLP4500.
I intended to display 128 images of 24 bit-width with pattern sequence mode (variable exposure). The images were fed from the video port, so I think they didn't occupy any space in the on-board flash. However, for the channel configuration (.ini file), the manual suggests the default maximum number of images [DEFAULT.PATTERNCONFIG.NUM_ SPLASH] should range between 0 to 63, namely only 64 images accepted by the system.
I'm wondering whether there's a method to increase the limit of this number by adjusting some parts of the board configuration. In case not, I'd also like to know if there's another practical way to implement such a substantial number of images. We're doing a set of sequential measurements, so we prefer not to separate the images into 2 or 3 sets but consider them as a complete set.
Thanks and regards,
Hank