This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPC7540: DLPC7540 Disp external mode brightness issue

Part Number: DLPC7540
Other Parts Discussed in Thread: DLP650TE,

Hi!

I have a DLP7540 and a DLP650TE  with firmware 4.5.0  dlpc7540_p65_udh_lpcw.dlpxproj.

Now I have  a brightness issue, the brightness of the Disp external mode white color is about 30% lower than that of the curtain mode.

The color coordinates of other RGB monochromes are normal. 

   

I would like to know which parameters to modify to increase the brightness of the Disp external mode?

Thanks!