Hello everyone,
I have some trouble in using my DLP3010 projector.
When running trigger in mode, I used a camera to trigger the DLP3010 projector with internal pattern。
At first, the projector is working correctly. But after more time, perhaps a few hours, the projector stop display the internal pattern.
Now I still could connect and operate the projector and the test pattern or splash is displayed correctly. Only the internal pattern could not be displayed, whatever the trigger in mode or the free-run mode.
The frame rate of the camera is about 80fps. The DLP3010 projector exposure parameters is as below picture.
So I am not sure whether the DLP3010 system unable to work stably for long time or there is a problem with my setting.
Thanks for any help.
Regards,
Yang