Other Parts Discussed in Thread: DLPA2005, DLPC3478
Hi Experts,
Recently I need to test the 1-bit monochrome pattern display with DLP3010LCFQK working in external pattern streaming mode.
The DLPC Write Pattern Configuration (96h) is shown as below:
(1) Sequence Type:1-bit mono
(2) Number of Patterns within each VSYNC_WE: 3
(3) Illumination Time: 2555 us
(4) Pre-illumination Dark Time: 171us
(5) Post-illumination Dark Time: 41us
Condition 1(The needed condition): When VSYNC_WE signal is triggered at 83.7Hz, DLP3010LCFQK is not projecting light and TRIGGER_OUT_2 always stays inactive.
Condition 2: When VSYNC_WE signal is still triggered at 83.7Hz with only "Sequnce Type" changed to 8-bit mono, DLP3010LCFQK is projecting light and TRIGGER_OUT_2 worked well.
Condition 3: When VSYNC_WE signal is still triggered at 83.7Hz with condition 1 config(sequence type: 1-bit mono), DLP3010AFQK is projecting light and TRIGGER_OUT_2 worked well.
The firmware version for DLPC3478 is 8.0.1 (Firmware name: FWSel_DLPC3478_DLPA2005_pm2_i2c0x36_v8p0p1).
Could you help me to solve this issue?
Thank you in advance for your support.
Best Regards,
Gavin