Hello,
i have the same problem as my predecessor I flashed the firmware but, nothing happened. Do you have a solution?
In the foto, you can sea what shows the terminal.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
i have the same problem as my predecessor I flashed the firmware but, nothing happened. Do you have a solution?
In the foto, you can sea what shows the terminal.
Hello User,
The team is investigating this behavior. when we find an answer I will close this thread and point you to the other thread for the answer.
Regards,
John
Thank you for your response.
We have a deadline on Friday. Is it possible to solve this problem by this term?
Regards
Šimon
Hello User,
The team is looking into this behavior and will get back to you as soon as we can.
Thank you for the patience!
Regards,
Lori
Hello User,
I want to clarify that the FPGA flash worked but the init_parallel had failed?
Can you go to the /dev folder and tell me if you have ether file i2c-1 or i2c-22? Can you confirm that the i2c.py script from the TI python support package is still present? Ideally you match the value inside the i2c.py script to 22 or 1. I am using 22.
Thank you,
John
Sorry that I didn't write you until now. i2C-0 and i2c-22 are present in dev. i2c.py I have in my DLP folder the same folder as init_paraller. I tried to change the number at i2c.py to 1,20,21,22 and parallel mod failed every single time.
Thank you
Šimon
Hello Simon,
What activity do you see on the D_HOST_IRQ LED? Ideally this would drive high for a moment during boot initialization and then drive low. Also, do you see any light output from the EVM?
Can you confirm that the I2C interface is enabled on the Raspberry Pi? You may need to go into the Raspberry Pi configuration to check.
Regards,
Austin
Hello Austin,
I filmed what the projector du during loading Firmware. Down in a video. When I initialized parallel mode then just the field and projector doesn't seem like something changed.
I2C is in the Raspberry Pi Configuration market as ON. I have one small hint I do not youse your private config.txt because mi Rasberi doesn't start whit them.
It starts but shows just a rectangle picture of color on the HDMI port and nothing else.
Regards,
Šimon
Hello Šimon,
Please try to use the default config.txt file.
The config file timings are compatible with the EVM init parallel mode. They are not typically compatible with monitors.
Please let us know if you have any problems.
Regards,
Lori