Other Parts Discussed in Thread: DLP3010
The DLP3010 hardware company provided me with the dlp3010 hardware and the dlpevm gui, and I needed to project several sets of 720 by 720 stripe patterns.
I connected the hardware in Advanced > Connection > CommandInterface in the gui, indicating that the connection was successful. Then in "Advanced "->" Commands"->"Display" set InputImageSize to 720, 720, ImageCrop to 0, 0, 720, 720, DisplaySize to 0, 0, 720, 720, There are no errors in EventViewer, and clicking Get in the appropriate place is no problem. After I powered off and restarted, when I added a set of 8-bit vertical patterns to LightControl -> InternalPattern ->"PatternSets" and added the 720 * 720 vertical stripes, the message "Image width does not match the display size" is displayed.Restarting without power off is the same error.
May I ask where I set the wrong, and how I need to operate to project the stripe pattern of 720*720?