I am trying to add images into the flash memory following section 3.9.1.2 of the manual. I follow the steps and is able to see the images. However if I try to examine the images currently in the firmware based on section 3.9.1, I don't see the correct image on the DMD. Also, the image does not change as I go through the different image index and I did not get any error message that says that the image does not exist even if I choose the 255 index.
I used the firmware 'DLPR900PROM — DLPC900 Configuration and Support Firmware' from https://www.ti.com/tool/DLPR900#downloads. Did I use the wrong firmware or did something wrong? The image on the left is the image on the DMD in video mode, the image on the right is the image I see on the DMD if I try to examine the images stored in the firmware.
I also have a question following Section 3.6.3 after adding images to the firmware. According to that section, I will choose Pre-Stored Pattern and continue with step 3 in Section 3.6.2. Step 3 in Section 3.6.2 is to add images from the computer. What does it mean to add images from the computer? I thought the Pre-Stored Pattern mode is displaying images that are stored in the flash memory of the controller?