Hi everyone.
We have design a custom board using DLPC3435 and DLPA2005 to drive a DLP .2 WVGA.
We haven't implement a USB to I2C or SPI on the board.
So in order to debug, flash the firmware in the Flash memory we wanted to use the DLP EVM GUI software. But I will need a USB to SPI/I2C converter.
From what I've read on this forum it appears that the GUI software is only compatible with few converter and one of them is not available anymore. (
So here is my questions:
- Can I use the CYUSBS236 from cypress ?
- Could the GUI use some serial command through an Arduino to connect to I2C ?
- Is there any documentation in order to create the code for an Arduino to do the job and make it compatible and usable with the GUI software ?
- Is there another way or procedure to flash the firmware on the flash memory ?
Thanks in advance for you help.