This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP4500NIR: Is it possible to control on, off and parked state for each pixel individually

Part Number: DLP4500NIR
Other Parts Discussed in Thread: DLPC350

As I know, DMD pixels could be parked by project control via composer, but the parked state can not be set for each pixel individually.

Is it possible to control and set on(+12°), off(-12°) and parked(0°) state for each pixel individually?

If yes, how to achieve that? Does it available in project control or need to modify source code?

If DLP4500NIR does not support this function, is there any other DMD product support that?