Other Parts Discussed in Thread: DLPC7540
Hi,
I am a bit confused about how to use the DLPC7540EVM. If I want to send an I2C command do I need some additional hardware connection or can I send the command over USB?
What I am trying to do is set the EDID setting in the front end EEPROM but I am unclear on how to do it:
I2C_CONFIG: 0x01 0xa0 0x86 0x01 0x00
I2C_PASSTHRU: 0x11 0x00 0x01 0xa0 0x00 0x00 0x00 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0x00 0x11 0x90 0xC9 0x02 0x00 0x00 0x00 0x00
DELAY : 0x05 0x00 0x00 0x00
I2C_PASSTHRU: 0x11 0x00 0x01 0xa0 0x00 0x10 0x15 0x18 0x01 0x03 0xA2 0x5A 0x37 0x00 0x1B 0x04 0x85 0xA0 0x57 0x4A 0x9B 0x26
DELAY : 0x05 0x00 0x00 0x00
I2C_PASSTHRU: 0x11 0x00 0x01 0xa0 0x00 0x20 0x12 0x50 0x54 0x5A 0xB4 0x80 0x31 0x40 0x61 0x40 0x81 0x3C 0x81 0x00 0x45 0x40
DELAY : 0x05 0x00 0x00 0x00
I2C_PASSTHRU: 0x11 0x00 0x01 0xa0 0x00 0x30 0x45 0x7C 0x61 0x7C 0x01 0x01 0x02 0x3A 0x80 0x18 0x71 0x38 0x2D 0x40 0x58 0x58
DELAY : 0x05 0x00 0x00 0x00
I2C_PASSTHRU: 0x11 0x00 0x01 0xa0 0x00 0x40 0x45 0x00 0x80 0x38 0x74 0x00 0x00 0x18 0x00 0x00 0x00 0xFD 0x00 0x1E 0x78 0x0A
DELAY : 0x05 0x00 0x00 0x00
I2C_PASSTHRU: 0x11 0x00 0x01 0xa0 0x00 0x50 0x73 0x0D 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0xFC 0x00 0x44
DELAY : 0x05 0x00 0x00 0x00
I2C_PASSTHRU: 0x11 0x00 0x01 0xa0 0x00 0x60 0x4C 0x50 0x36 0x35 0x30 0x30 0x20 0x48 0x44 0x4D 0x49 0x20 0x00 0x00 0x00 0x10
DELAY : 0x05 0x00 0x00 0x00
I2C_PASSTHRU: 0x11 0x00 0x01 0xa0 0x00 0x70 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x01 0x7D
DELAY : 0x05 0x00 0x00 0x00
I2C_PASSTHRU: 0x11 0x00 0x01 0xa0 0x00 0x80 0x02 0x03 0x1C 0x00 0x4C 0x90 0x1F 0x22 0x29 0x2F 0x02 0x11 0x04 0x30 0x2A 0x2B
DELAY : 0x05 0x00 0x00 0x00
I2C_PASSTHRU: 0x11 0x00 0x01 0xa0 0x00 0x90 0x01 0x66 0x03 0x0C 0x00 0x11 0x00 0x00 0xE3 0x05 0x1F 0x00 0x00 0x00 0x00 0x00
DELAY : 0x05 0x00 0x00 0x00
I2C_PASSTHRU: 0x11 0x00 0x01 0xa0 0x00 0xA0 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00
DELAY : 0x05 0x00 0x00 0x00
I2C_PASSTHRU: 0x11 0x00 0x01 0xa0 0x00 0xB0 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00
DELAY : 0x05 0x00 0x00 0x00
I2C_PASSTHRU: 0x11 0x00 0x01 0xa0 0x00 0xC0 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00
DELAY : 0x05 0x00 0x00 0x00
I2C_PASSTHRU: 0x11 0x00 0x01 0xa0 0x00 0xD0 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00
DELAY : 0x05 0x00 0x00 0x00
I2C_PASSTHRU: 0x11 0x00 0x01 0xa0 0x00 0xE0 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00
DELAY : 0x05 0x00 0x00 0x00
I2C_PASSTHRU: 0x11 0x00 0x01 0xa0 0x00 0xF0 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0xFF 0x41
DELAY : 0x05 0x00 0x00 0x00
Thanks for your help.
Paul